This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK1C1104: sinewave input/maximum input slew rate

Part Number: LMK1C1104

I would like to use the LMK1C1104 with either an LVCMOS or sinewave input at 40MHz. With a 3.3V supply, what is the MAXIMUM input slew rate, i.e., will it work with a sinewave? The data sheet only specifies minimum slew rate. 

  • I think I misstated this question. What is the maximum input RISE TIME (inverse of slew rate). If I read the data sheet correctly, a minimum slew rate of 0.1V/ns implies that my 40MHz sinewave won't work with this part. Am I correct?

  • Hi Barry,

    The slew rate specification is for 20% to 80%.  So a sine wave actually does get moving well enough here that at 40 MHz you can meet the slew rate specification.  For example:

    40 MHz @ 3.3 V from 20% to 80% is 0.387 V/ns, risetime = 5.1 ns
    40 MHz @ 2.5 V from 20% to 80% is 0.293 V/ns, risetime = 5.1 ns
    40 MHz @ 1.8 V from 20% to 80% is 0.211 V/ns. risetime = 5.1 ns

    As for maximum rise time, since we specify slew rate, the maximum allowable rise time becomes a function of amplitude.  The larger amplitudes have longer allowed rise times.  In my example above, the slew rate increases because I hold the frequency (which is associated with rise time) constant while increasing amplitude.
    So for a 3.3 V signal, a 10.5 MHz sinewave would have just over a 0.1 V/ns slew rate with a rise time of 19.5 ns.
    For a 1.8 V signal, a 19 MHz sinewave would have about 0.1 V/ns slew rate with a rise time of 10.8 ns.

    Of course supply isn't always exactly 3.3 V or 1.8 V.

    Hope this helps.

    73,
    Timothy

  • Thanks, Timothy.

    I wasn't thinking quite clearly (apparently) when I posted this. This makes perfect sense.

    TU,

    Barry