I make sure the chip in fallback mode by set REFSEL and EEPROMSEL float.
1. Then register commit first step, said pre-configure hardware or chip register? Does this step mean to set register 0.bit0 to 1 through I2C bus? If so, can the coming steps next continue to use I2C bus normally?
2. Should I write the registers with value through I2C bus first, then execute these Register Commit flow to copy to EEPROM? Any sleep to wait between some steps?
When it will finish the EEPROM programming? Just right after CRC written?
3. EEPROM access direct is also write 0x74 device, right?
4. When 0x76 and 0x77 device address will be using? Only if the hardware configuration takes effect, but not disable serial interface, set register 0. bit0 = 0, not 1, right?
Only in this case, user can use 0x76 or 0x77 access the EEPROM directly, right?