SIT3808AI-CF-33EM-50.000000X as VCXO and the DSC1101DL5-050.0000 as CLKIN1.
we have failed?LMK04610_2021b.tcs
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ed,
This sounds like either an issue with the switch between fastlock coefficients and final coefficients, or the lock detection circuit is misbehaving.
Have you tried using the PLL1 loop filter tool page to set the bandwidth for PLL1? Try configuring the device for something like 20Hz and see what coefficients are recommended. I get much less proportional gain than what you are using. You could also try adding a small amount of integrator gain (1-2) to your current setup.
Have you checked that CLKIN and OSCIN frequencies are actually drifting in phase when the device reports unlock condition? If they are actually phase aligned, it may just be a lock detect reporting issue and we could look for configuration issues with lock detect.
Regards,
Derek Payne
Hi Derek,
Thanks for your answer.
It is a bit tricky to measure at the device (not accessible) so I can not provide you with phase details right away.
Could you provide me with the correct settings for PLL1 and if in case I am not really interested in the absolute
quickest way to "lock", could you provide me with the fastlock-settings that are "full-proof/fool-proof". To my knowledge, fastlock is not enabled
in our config. Regarding the lock detect, you have the configuration file and as far as I know the lock detect windows is at its "widest".
Anyway, if you could provide me with better settings for PLL1 I would appreciate it very much, then over the weekend I will try to connect some
wires for the signals that you have requested.
Kind Regards
Ed
For the
Hi Derek,
Thanks for your answer.
It is a bit tricky to measure at the device (not accessible) so I can not provide you with phase details right away.
Could you provide me with the correct settings for PLL1 and if in case I am not really interested in the absolute
quickest way to "lock", could you provide me with the fastlock-settings that are "full-proof/fool-proof". To my knowledge, fastlock is not enabled
in our config. Regarding the lock detect, you have the configuration file and as far as I know the lock detect windows is at its "widest".
Anyway, if you could provide me with better settings for PLL1 I would appreciate it very much, then over the weekend I will try to connect some
wires for the signals that you have requested.
Kind Regards
Ed
Hi Derek,
My apologies for not responding earlier.
I have been measuring over the weekend and concluded that the pull-range of the VCXO was too small.
Fortunately I could replace that one with a VCXO with a larger pull-range and that solved the
"lock-detect" problem. So in fact the lock-detect did exactly what it should be doing.
Thanks,
Ed