The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLLATINUMSIM-SW: Option menu tab

Part Number: PLLATINUMSIM-SW

Hi all

Would you mind if we ask PLLatinum SW?

There are options on the menu tab as follows;

.
Using these check box, we could not judge what settings or show are changed.
What are these settings used for?

Kind regards,

Hirotaka Matsumoto

  • Hi Matsumoto-san,

    In general, we don't need to alternate these options. When these options are checked, it will ensure all the calculation will be done automatically whenever a parameter is updated. The third option will reduce the PLL DEN and NUM to the lowest value. For example, in TICS Pro, when DEN = 1000 and NUM = 100. In PLL Sim, they will be reduced to DEN = 10 and NUM = 1. TICS Pro also has a button to reduce them to the lowest value. This option helps us identify possible spurs frequencies. For example, in this case, 1/10 = 0.1. We know that fractional spurs will appear at 0.1 * fpd.