This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214: Default data of EEPROM Page0 and Page1

Part Number: CDCE6214

Hi all

Would you mind if we ask CDCE6214?

Could you let us know default data of EEPROM Page0 and Page1?
On the other forum, there are default data of EEPROM Page0 and Page1.
e2e.ti.com/.../cdce6214-q1-default-setting-of-eeprom

So, are these data for 25MHz(input) with LVCMOS -> 100MHz(outputs) with LP-HCSL(in case of page0) or LVDS(in case of page1)?
Is our recognition correct?

As the back ground of this question, using TICSPro, when the tool has previous reference input data=48MHz, the output is 192MHz.
So, we would like to confirm just in case.


Kind regards,

Hirotaka Matsumoto 


  • Hi Hirotaka,

    The default reference frequency is 25MHz. I believe the default reference selection method is pin selection, meaning that pin REFSEL is used to decide whether to select PRIREF or SECREF. SECREF should be XTAL mode by default.

    Regards,
    Hao