・Is it okay to not need a 50Ω resistor on the OSCIN_P pin when inputting a CMOS clock to the OSCIN_P pin? Is it okay to input a 50MHz CMOS clock with high impedance?
・Reference Does the phase noise performance change depending on the input level of Oscillator Input? I want to check if the phase noise is dependent on the Reference level.
・Data sheet Figure 6-8. For Output Power vs. OUTx_PWR, is there a regulation for each power step of OUTx_PWR 0 to 7? (If the OUTx_PWR value is changed by 1, it changes by 〇 dB, etc.) Figure 6-8. Shows three graphs of OUTx_PWR = 0,4,7, but the power difference between OUTx_PWR = 0 and 4 and the power difference between OUTx_PWR = 4 and 7 are significantly different, so check the above. I want to