Hi there,
I am using the LMK04832 application with a SY89297U delay block. Is there any perceived issue with this combination? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I am using the LMK04832 application with a SY89297U delay block. Is there any perceived issue with this combination? Thanks
Hi Oscar,
There's no electrical reason preventing these two devices from working together - the output of LMK04832 should be compatible with the input stage of this delay block. However, the noise floor on the SY89297U is significantly higher than the LMK04832 (>30dBc/Hz). The total jitter with this delay block will be much worse than an output from LMK04832.
Regards,
Derek Payne