This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832-SP: Not Powering Unused Clock Groups

Part Number: LMK04832-SP

On the board I am designing, several of the clock generator outputs will not be used.

To save space (ferrite beads, decoupling caps, etc), I am wondering whether it is ok to not power these clock groups.

If for example, I do not need clock outputs 0, 1, 12, or 13, can I simply leave the output pins (CLKout*) not connected and do the same for the power pin (Vcc12_CGO)?