Other Parts Discussed in Thread: LMK00334
I want to choose between (3) LVDS clocks and level translate to 2.5V from 1.8V. The LMK00338 seems to be overkill but it level translates clock levels and selects the clock of interest. The three clocks are differential and are at 156.25MHz, 125MHz, and 100 MHz. Is there a better solution because I don't need to fan out the selected clocks?