The TI E2E™ design support forums will undergo maintenance from Sept. 28 to Oct. 2. If you need design support during this time, contact your TI representative or open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00338: Better solution to MUX and level translate 3 LVDS clocks?

Part Number: LMK00338
Other Parts Discussed in Thread: LMK00334

I want to choose between (3) LVDS clocks and level translate to 2.5V from 1.8V. The LMK00338 seems to be overkill but it level translates clock levels and selects the clock of interest. The three clocks are differential and are at 156.25MHz, 125MHz, and 100 MHz. Is there a better solution because I don't need to fan out the selected clocks?