Other Parts Discussed in Thread: USB2ANY, LMX2594
I am measuring huge amounts of noise and spurs in the sidebands of a CW signal generated by the LMX2594EVM while I am connecting it with the Reference Pro board (SV601349). I have tried several frequencies including the supplied default of 7GHz and also 11.7GHz which is what I ultimately want.
1. I located the source of most of the noise. It is coming from the Reference Pro board (SV601349) board. When I place a piece of ferrite on top of the IC the noise is reduced by more than 20dB. What is causing this on the reference Pro board?
2. I then substituted an older interface supplied with with a different EVM. It is the USB2ANY module. It loads the LMX2594EVM correctly from TICS and has far lower noise. However, now there are a few large spur signals in the sidebands of the microwave signal from the LMX2594EVM. One is at 2.5KHz away from the carrier and is only 20dB down from the carrier level. What is causing this?