Hi team,
One of our customers has the following needs:
Give Trig1、Trig2 or MOD pin a trigger signal of a rising edge, and then the chirp signal starts to be sent. The cycle of a chirp is 60us. I send the trigger signal every 100us, and a chirp will be generated.
Method: MOD_PIN[2:0] configured as input, MOD_MUX[4:0] is configured as Input MOD; Start next ramp after select Trigger A, RAMP_TRIGA[3:0] is configured as
MOD terminal rising edge
Question: after configuration, the radar only generates a chirp signal, and then a single tone signal that is always the initial value. Is there a problem with my configuration?
Best Regards,
Amy Luo