Hi. I have fabricated LMX2615 and interfaced it with Refpro Board. Initially I got the output well. But later on after few days there was no output. I have monitored the voltage levels through out the board and every thing is fine but only at one pin that is mainly on CSB pin. The Voltage is 0.017V instead 3.3V. Could anyone please help me to debug the issue. The spi Lines I have connected are SDI, SCK, CSB, GND.
Thank you in Advance