This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE913PERF-EVM: Dimension/3D file

Genius 9880 points
Part Number: CDCE913PERF-EVM


Hi,

Customer is looking for the 3D/Step file or dimension of CDCE913PERF-EVM?

Can TI provide the files?

Thank you in advance.

Regards,
Maynard

  • Hi Maynard,

    It's been a while since anyone looked at this EVM, so we're looking for the board files. I'll make an update once we have more to share.

    Regards,

    Derek Payne

  • Maynard,

    The file was done in OrCAD, and we've since moved to mostly Altium. It took a lot of finagling just to get the board file working again, but I have some board dimensions (in mils):

    Board X/Y: (-125, 2875) to (3875, -125)

    Mounting Holes 150mil dia at (25, 2725); (25, 25); (3700, 2725); (3700, 25).

    In other words, there's 150mil between each board edge and the center of the 150mil dia mounting holes, and the board itself is 3in x 4in.

    I'm not very knowledgeable about OrCAD/Allegro, so I'll include the design file in case you can extract more usable information out of it than I can.

    CDCE913PERF-EVM-Layout.brd

    Regards,

    Derek Payne