Other Parts Discussed in Thread: USB2ANY
Hi,
Good day.
Our customer has inquiry about the LMX2595 . Kindly see below.
I am trying to program the LMX2995EVL via the SPI (with an micro-controller board) to just generate any frequency, but it is not working.
I check the trams with an oscilloscope and it is correct according to the datasheet. All the register values that I tried to send to the LMX2595 are from the TICS pro software made by TI so it should be the right ones. The hardware looks also correct because I took as an example the LMX2995EVL working with the TICS Pro to check the signals sent between them.
The only thing that seems not right is that the Lock LED is off, even if the value of MUXOUT_SEL is set to 1 (lock detect). I suppose the values of my registers are not correct to obtain a lock state but they are from the TICS Pro software so it does not make sense to change them.
I hope you could help me and I wish you a pleasant day.
Can you please help us? Thank you.
Regards,
Cedrick