Other Parts Discussed in Thread: LMK00334
Hello,
Q1) Are all 4 outputs of the 2 banks on LMK00334RTVRQ1 in sync?
Q2) This chip could have 4 outputs in HCSL format and I need to drive two HCSL receivers and 2 LVDS receivers, all in sync.
Based on HCSL output and LVDS input circuits it sounds to me I can ac couple the HCSL outputs to LVDS inputs w/o any issues, taking into consideration that my LVDS receivers have 100Ohm termination and biased internally at 1.2V. Could you please confirm this for me?
Thanks,
Reza