Other Parts Discussed in Thread: LMX2595
Simulator does not seem to be usable for the LMX2595.
When I use Interface with TICSPro to import .tcs file all of the settings are imported successfully, but the simulator seems to be dead. All of the results tabs (phase noise, spurs) are frozen in the states they were in before the import. I have to close and restart PLLatinum to get it working again.
Manually entering the configurations is like playing whac-a-mole. For example, I want:
Fosc=100
input multiplier=2
Fpd=240
Fvco=14000.01
Fout=7000.005
output divider=2
I can't get all of these simultaneously.
output divider keeps changing to 1.99 or Fvco changes to 14000.00256, or Fout will change.
I can't manually enter feedback divide because there does not seem to be a way to enter integer part. Is it expecting improper fraction for Fnum?
Its a little irritating that Fnum & Fden do not accept cut/paste (for example from TICSPro).
The integer boundary spurs are in the wrong places, but I assume this is because the configurations are not what I want.