This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: CDCI6214 Configuration

Part Number: CDCI6214
Other Parts Discussed in Thread: LMX2572

Hi Team,

I use the TICS PRO to help customer modify the configuration of CDCI6214 (provided by TI 2 years ago), when I import the hex register configuration, it shows the error below. I click YES, but see nothing to change. I am not sure if there has some issue from my side. So, could you help look at the attached TXT configuration file and modify all outputs from previous 100MHz to 50MHz? thanks a lot.

Best regards,

Yang

CDCI6214 2x100 2x160 2020-3-24 LVPECL.TXT