Hello,
When looking at the registers for the LMX2592, should I assume that that the TICS pro has the newest register fields and updates? I noticed discrepancies between the datasheet listed under the technical documentation and the TICS pro application and would like some clarification on the right fields.
Registers 11, 12, 37, 38, 40, 41, 44 & 45 have fields listed on datasheet, but no fields within the TICS pro under the Raw Registers tab within the Context section.
R30: In TICS pro, PLL tab lists vco doubler as Register 30 field (Which lines up with the field listed in datasheet at bit zero) but the Raw registers tab doesn't list the field and instead has a VCO_BAND field not listed in datasheet.
Data sheet:
TICS PRO:
PLL tab-
Raw registers tab-
For R13, field PFD_CTL, different bit mappings are present.
TICS Pro: bits 0-11
Datasheet: bits 8-9
Thank you for your time.
-Andrey