Hi,
i'm a bit confused regarding the Fcal_en bit, can i work with the synt when its low?
we work at freqs in VCO2, after configuring via SPI on our board the freq as we did on the EVB, we see that the frequancy repeatdly moving, we noticed when we turn off this bit to '0' it stays constant and stable.
maybe we do somthing wrong? just to notice we use the vco/phase sync thus i guess we must that this bit be on. should it be on all the time? or only during sync.
its seems like as if the vco callib procefure is working repeatadly during this bit on state and thus our vco moving and not stable.
in the video you can see how it becomes stable after we set Fcal_en to '0'