This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00725: Termination for HCSL output to input of LMK00725

Part Number: LMK00725

Hi, I have an HCSL output (NB3N5573) that I want to use to drive the input of the LMK00725, that should accept HCSL.

I can't see any guidance on the termination needed to match the LVPECL, LVDS, HCSL, SSTL, LVHSTL compatible input of the LMK00725 to an HCSL signal.

Can you provide a recommended termination method?