Hi,
I have a question about SYNC category for LMX2594. In my design, I used 1xLMK04828B + 4x LMX2594. Multi-chip synchronization is needed to sync these 4pcs LMX2594.
In my setup of LMX2594 as below figure1 shown, RFoutA will output 10GHz as device clock and RFoutB will output 4.8828125MHz as sysref clock for high-speed ADC. So output MUX for RFoutA is switched to VCO, and output MUX for RFoutB is switched to SysRef.
My question is that
1. no channel divider will be included into the path of RFoutA, so I only choose the path as marked red in figure2 ?
2. Category1 will be the last result, and it mentioned "SYNC Mode Not required at all". That mean SYNC mode couldn't be used?
figure1 . setup of LMX2594
figure2 . SYNC category
Best regards!!!
Jason