This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2541: Default register settings at power up unclear

Part Number: LMX2541


We are using the LMX2541SQ3740E and discovered the following strange behavior:


At power up the state of the pin 20 (Ftest/LD) is not well defined. We have installed a 1k Ohm pull-up to 3.3V on this pin.
If not configured some devices show a high level others a low level on that pin.
After the configuration the MUX register (MUX[3:0] = 4), everything is fine.
Now my question, what is the power up state of the MUX[3:0] register, I do not find any information in the data sheet (SNOSB31J –JULY 2009–REVISED DECEMBER 2014). For some registers, the default state is mentioned in the data sheet.

Are all not mentioned registers set to zero at power-up? 
If, yes MUX[3:0] would be 0, which means "High Impedance", but then it should not be possible to have different power levels if the chip is not configured. It should always be a high level.