Other Parts Discussed in Thread: LMX2594, ADS54J64EVM, LMX2572, LMX2491, LMX2492
We are working on a prototype for an automotive sensor that works at MMW frequencies. Here are some of the questions I have in mind:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are working on a prototype for an automotive sensor that works at MMW frequencies. Here are some of the questions I have in mind:
Hi Abdulrahman,
If you are looking for linear frequency ramping with 500MHz ramp range, LMX2594 or any synthesizer with built-in VCO is not a good choice. You need to use discrete PLL, such as LMX2491 or LMX2492, + external VCO. LMX2594 can support approx. 100MHz linear frequency ramp range. A higher ramp range will requires a VCO calibration, as a result, the ramp is not linear but a staircase ramp. For details, please read LMX2572 datasheet.
Please post ADC questions to the Data Converters forum.
Thank you Noel for directing me toward the right board.
If I go with the LMX2492.
- Can it chirp over the 500MHz in 10 micro-sec?
I appreciate your helping with these questions.
Hi Abdulrahman,
From the device configuration point of view, it is possible to ramp 500MHz in 10µs.
In practice, the loop bandwidth should be wide enough or otherwise we may not get linear ramp.
LMX2492 is typical analog PLL. During ramping, the internal ramp engine will increase PLL_NUM and PLL_N to change (external) VCO frequency. If the VCO frequency is an integer multiple of the PLL reference clock, I think the phase between VCO and reference clock is deterministic. We never did phase measurement, we don't have any test data.
What trigger did you mean?
For the phase: if i want to generate a train of ramps (like a sawtooth signal) how can I insure that the starting phase of the starting frequency of each ramp is matched for all ramps? does it start the PLL reference clock for each ramp and at a fixed phase?
By trigger, I mean arming or starting the ramping. The time from point of sending the signal to start ramping until the ramp is at RF output, is this time deterministic?
Hi Abdulrahman,
I don't know the phase issue, our ramp engine changes the N divider value during ramp, we have never do any phase alignment. The ramp time is deterministic as the ramp is running at the phase detect frequency. For example, if fpd = 100MHz, the ramp engine will increment N divider once every 10ns.