This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLLATINUMSIM-SW: format for custom OSC input source / VCO noise and PLL noise

Part Number: PLLATINUMSIM-SW


Dear Team,

On the PLLatinum SIM ; Feature Level=Advanced , under the Phase Noise tab there is an option to "Load Data" for custom input OSC / VCO Noise / PLL Noise

Can you please share an example or a short guide on how to enter the data for custom OSC input source / VCO noise and PLL noise ?

Regards,

Nir

  • Hi Nir,

    Attached here is an example. The left column is offset frequency in Hz.

    100	-116.5
    1000	-134.7
    10000	-148.2
    100000	-157.2
    1000000	-161.3