This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5B12204: Single ended LVCMOS Output Level + 50ohm termination

Part Number: LMK5B12204


Hello all,

Assuming VDDO_x is 3.3V, what would be the single ended voltage swing (pk-pk) when driving a 50ohm termination?

Output frequency is 32MHz

I'm measuring about 1.1Vp-p with the above condition, is this what should I expect?

Thanks!

Nir

  • Hi Nir,

    The LMK5B12204 should have VDDO_x = 1.8 V for full swing LVCMOS outputs. Using VDDO_x > 1.8 V for LVCMOS would result in reduced swing outputs. I expect such behavior from your setup.

    Regards,

    Jennifer

  • Hi Jennifer,

    I've seen this data, it doesn't specify if the LVCMOS driver is terminated with 50ohm or not.

     

    Is this the way the measurement was taken? 

    Best regards,

    Nir

  • Hi Nir,

    I see your confusion.

    • The LVCMOS driver does not require 50 ohm termination. 
    • Yes, Figure 8-1 shows the test setup used to gather the LVCMOS spec in the datasheet. That is, using a Hi-Z probe.

    Regards,

    Jennifer

  • Hi Jennifer,

    Regarding the Hi-Z probe test condition - understood.

    By the way, the LVCMOS driver requirement for a 50ohm termination is per application.

    It's not whether the driver needs termination or not, it is depends on the trace length.

    For a relatively short trace length, it is ok not to put 50ohm termination at the receiver side - by doing so you get the full signal1.8V swing:

    If the trace is relatively long, this will cause signal reflection, then it is necessary to add termination - by doing so you get half of 1.8V swing (In my measurement I used 50ohm termination and measured about 1Vp-p signal swing):

    Best Regards,

    Nir