Hi,
The differential output peak to peak voltage in the datasheet is 0.5V to 1.35V. Looks like it is a full frequency range spec in datasheet figure 2. my application is 80MHz, the typical value shall be close to 1.2V. What is the variation range of this spec. i mean what is the min and max Vpp at 80MHz application?
The load chip is sensitive about the input power. So I wish the min output power of CDCLVP1102 at 80MHz is enough.
Regards,