This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE925: How to confirm the read set values

Part Number: CDCE925

Hello,

The following is a reading of the setting values normally used in the CDCE925 that the customer is using.

CDCE925.HEX.txt
:01000000817E
:0100010008F6
:01000200B449
:0100030003F9
:0100040002F9
:0100050050AA
:010006006099
:0100070000F8
:0100080000F7
:0100090000F6
:01000A0000F5
:01000B0000F4
:01000C0000F3
:01000D0000F2
:01000E0000F1
:01000F0000F0
:0100100000EF
:0100110000EE
:0100120000ED
:0100130000EC
:010014006D7E
:0100150002E8
:0100160002E7
:0100170008E0
:01001800FFE8
:010019008066
:01001A0002E3
:01001B0007DD
:01001C0000E3
:01001D0040A2
:01001E0002DF
:01001F0008D8
:0100200000DF
:0100210000DE
:0100220000DD
:0100230000DC
:010024006D6E
:0100250002D8
:0100260001D8
:0100270005D3
:010028009F38
:01002900B026
:01002A0002D3
:01002B00894B
:01002C0000D3
:01002D004092
:01002E0002CF
:01002F0008C8
:00000001FF

Is there a way to check the settings on TI Clock Pro S/W with this file?

When the customer imports the file, it is displayed as below.

Could you please tell us which values match the settings in the file?

Thank you.

JH

  • JH,

    The "Bit Viewer" button on the left side of the GUI screenshot that you provided can be used to determine if the settings are correct. The registers and corresponding data should match up to what is seen here.

    From the second to last line of the file that you attached: 01 00 2F 00 08 C8, the register is the third byte, and the data is the fifth byte.

    In terms of which values match which registers, the register map is discussed on page 19 of the datasheet: www.ti.com/.../cdce925.pdf

    Thanks,

    Kadeem