This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2694-EP: skew output some phase degrees?

Part Number: LMX2694-EP

Hello,

Quick question about the LMX2694.  It looks like you can skew the output some phase degrees.  Is that correct?  I have one application that generates a 2.5GHz output from a 625MHz input.  I need to be able to shift this output +/- 10ps (i.e 0-45 degrees).

Is this true for both the -EP and -SEP versions?

Thanks,

Adam

  • Hi Adam,

    We can use Equation 5 to determine the amount of phase shift.

    With below configuration, the phase shift is 9 degrees every time your program R41 with MASH_SEED = 100.

    Both EP and SEP support this function.