Hello,
I am running the input SI simulation for the LMK1D1204 as shown in Figure 8-4 in the datasheet. The driver is an LVDS driver with 50ohm termination to VAC_REF after the blocking caps. When running a TDR measurement I am seeing unexepected transient behavior. Can TI run the IBIS on the input at 100MHz to see if there is an issue with the model or with my setup?