Other Parts Discussed in Thread: USB2ANY
Hi!
User guide for CDCE6214-Q1EVM explains how to set up the board for external 5V power, but it requires modifying the board and I don't really see the need. What I would like to do is use the USB connection to power up the board but connect an external FPGA i2c ports to the device's. Is this possible somehow?
Also, regarding this, the user guide is a bit confusing, as it says:
Short pins 2 and 3 of J6 and pins 2 and 3 of J10. The purpose is to disconnect the SDA and SCL pins
Connect SDA (pin 2 of J6), SCL (pin 2 of J10), and GND to USB2ANY.
But of course I cannot do that because there is a jumper on pin 2 of J6 (which, by the way, are not numerated, so there's no way to know which is which)
Thanks!