This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK1C1104: LMK1C1104 - different voltage levels for input vs. output

Part Number: LMK1C1104

Hello. Can you please confirm that it is not a problem to use a 3.3V LVCMOS signal on the input clock when VCC=1.8V? There is no maximum specified in the datasheet for VIH, which leads me to believe that the "absolute" max of 3.6V is the threshold, but I would like to confirm.

Thank you.

Regards.