Other Parts Discussed in Thread: LMK00334, CDCDB400
Hello,
I need to split one PCIE3 clock of one 8 lanes bus to two clocks each for 4 lanes bus.
Can LMK1D1204 be used in order to split PCIE clock to 2 clocks ?
I'm asking that since PCIE3 is routed with 85 ohms impedance and the LMK1D1204 says its split clocks shall be terminated with 100OHM.
Therefore I wonder if it is OK to use it to split the clock and if I do so than shall the 100ohm parallel termination on the device input shall be replaced with 85ohm ?
Thanks and BR,
Ohad