Other Parts Discussed in Thread: CDCM6208,
Hi!
I have a question as title.
As I read past thread;
There is description about application report (https://www.ti.com/lit/an/scaa059c/scaa059c.pdf),
but I'm still not clear about differential input termination.
I consider about which circuit attached image below is better AC coupled LVDS with CDCM6208 for 2 types.
Type (1) is 2 AC coupling capacitors and 50 ohm termination for both positive and negative line.
Type (2) is 1 AC coupling capacitor for both positive and negative line and 100 ohm termination across the line.
Mother board is already mounted, and I want to use type (2) to decrease the parts.
I think type(2) will work, but I wonder there is any problem;
As CLKin and CLKin* is pre-biased about 1.4V, something wrong occur because of some difference of pre-biased voltage between CLKin & CLKin*.
If there are no problem, I want use type(2).
Best Regards,
Naoyuki