This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00334-Q1: HCSL Voh voltage a little bit small

Part Number: LMK00334-Q1

Hi team, 

According to the datasheet, min value of Voh is 520mV, which  is a little smaller than customer required. 

There should be a 15mA current in the driver stage of HCSL output, which means there should be 15mA*50ohm=750mV in output, why the min value is so small? If it is caused by test, please share test setting(for example, Rs value). If it is caused by variation between different devices, please share the Distribution of this specs to help me convince customer. 

B&R

Lijia