What should be the value of the resistance in the red box?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'll add that the structure of the LMK11xx LVCMOS output buffer actually includes a series resistance built into the output stage that is designed to complement the impedance of the driver FETs to make a nominal 50Ω impedance. This diagram is likely copied from a previous LVCMOS buffer that did not include a series resistance in the output stage, where the output impedance might have been closer to 25Ω - in these cases a series resistance of 22Ω, 27Ω, or 33Ω might have been suggested to help match 50Ω source impedance. LMK1106 and other similar-family LMK11xx parts do not require a series resistance, and that component may be omitted.