Hi Expert,
my customer is using LMK00105, the output current for VDDO in D/S 3.3V supply is typ 7 mA. do we have any max limitation, the application shown as below will reach to 35mA for each output.
in other E2E list, I see that if we don't have max or min value in the datasheet, it means we don't measure the limitation, so only show typical value as customer's reference. is it also could be used here? thansk.


BR
Chi