This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLLATINUMSIM-SW: Starting software error

Part Number: PLLATINUMSIM-SW

Hi TI support,

I have an error when open the PLLATINUM SIM software (French version) . So I can't acces to the soft for simulate parameter of the LMX PLL.
Do you have an idea to resolve this error ?


Best Regards.

  • Hi,

    The first thing I would try is to dlownload version 1.6.3 from ti.tool/pllatinumsim-sw

    We had this issue before, but it should be fixed.

    This is related to the switching of "," and ".".   In other words, "1/2" = "0.5" in english format, but in other languages, "1/2" = "0,5".  This is causing an issue when the database is loaded.  

    To test this, we go to the control panel in the regional settings and make it so that "," is the decimal point and "." is the numerical separator.  

    So in summary, try downloading version 1.6.3 and see if this fixes your issue.

    Regards,

    Dean