This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK01000: Too many VCC. What are the diferences?

Part Number: LMK01000


Hello E2E Experts,

Good day.

1. May I ask what are the differences between different VCC names? VCC1, VCC2..., etc.

2. Is it internally connected?

3. What is the reason behind many bypass capacitors for each Vcc pin?

Regards,

CSC

  • Hi,

    The VCC are not internally connected, but you supply the same voltage to them.

    May of these are to supply different outputs.  In the case that the outputs are running at different frequencies, it is good to have some isolation and decoupling for these.

    If all the outputs are the same frequency, then this isolation is less critical and you can short them together.

    If they are different frequencies, then it is better to isolate them to get lower crosstalk between outputs.

    On our evaluation board, we put bypass capacitors everywhere to cover the worst case scenario of all outputs at different freuqencies