Hello Community,
We're working on a project that involves transmitting a 32kHz clock signal from a MEMS TXO (SIT1552AC-JE-DCC-32.768E) to a remote MEMS Accelerometer via a 2-3m CAT5e Cable. We plan to use AM26C31/32 differential driver/receiver for this.
- Can the clock output be directly interfaced with the AM26C31, and can the AM26C32 output be connected to the MEMS Accelerometer's CLKIN pin?
- Are there alternative methods for transmitting a 32kHz clock signal effectively?
Your guidance would be greatly appreciated.
- Clock Source is SIT1552AC-JE-DCC-32.768E
- Differential Driver is AM26C31
- Differential Receiver is AM26C32
Additionally, we have a concern about installing the MEMS TXO on the same PCB as the MEMS Accelerometer. The setup will be exposed to 1g vibration across DC to 1000Hz, with spikes up to 4g.
- Is it advisable to have the MEMS TXO onboard on a vibrating equipment given its MIL-STD-883 70g certification?
- Or should we consider installing the MEMS TXO on an external PCB and transmit the clock signal over differential signal to improve reliability?
Your insights would be highly valuable.