Hi Team,
This is technical support request for CDCI624. When CDCI6214 PLL unlock occurs, except for powering off and restarting, no matter how you configure the chip or RESET, it cannot return to normal. After merging the i2c of the CDCI6214 EVM development board into the chip and configuring it, the phenomenon remains the same. At this time, except for Y0 which can output normally, the other channels cannot output normally if different configurations are selected.
When used CDCI624 for PLL parameter calculate, we selected custom since there is no CDCI624 option in PLLatinumSimm for device selection. Is that correct like below picture shown?
The Phase-Locked loop Circuit in below picture is not the similar with the CDCI624 internal, is it will unavailable?
William