Other Parts Discussed in Thread: CDCI6214, CDCI6214EVM
Hi,
I am using the LMK03318 to generate several differential outputs. But the output7 peak to peak swing is always larger than other output. The swing is almost about 2V that is larger than the maximum 1.6V spec too. The configuration of these outputs in TICS Pro are same.
Below are the schematic I am using. I measured the clock before the ac-coupling capacitors. So if believe the output swing should be same, no matter what the load is used after the capacitors.
Output7:

output 0, 2, and 5. the waveform are similar, only upload one.