help to review schematic,how to terminaed about LPHCSL output(Add seried resistors,ac caps?),thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
help to review schematic,how to terminaed about LPHCSL output(Add seried resistors,ac caps?),thanks.
Peter,
Typically 0-Ohm resistors are placed in series with the output clocks to allow for swapping out with a different value for better impedance matching or amplitude attenuation.
Ensure that REFSEL is pulled low to select SECREF as the input clock.
We recommend using an additional ferrite bead + capacitor for isolating VDD_VCO from the other VDD domains.
Thanks,
Kadeem
thanks ,
1.when use SECREF as clock,how to deal with PRIREF pin 5 and pin 6?
2.For clock output connecto to SSD(MTFDHBL128TDQ-1AT12ATYY) PCIE ref clock,do we need to add 100ohm at SSD side?
Peter,
The PRIREF pins can be left disconnected when only SECREF is used.
The outputs of the CDCE6214-Q1 are LP-HCSL rather than HCSL, so 50Ohm termination resistors to GND are not needed.
Thanks,
Kadeem