If setting VCXO frequecny 122.88MHz and the VCO1 frequency 15099.494MHz, but the actual VCXO frequency is 20MHz, will the actual VCO1 frequency be 2457.6MHz? What's the potential risk it will be ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If setting VCXO frequecny 122.88MHz and the VCO1 frequency 15099.494MHz, but the actual VCXO frequency is 20MHz, will the actual VCO1 frequency be 2457.6MHz? What's the potential risk it will be ?
Daniel,
From my understanding you require PLL2 to support a VCXO frequency of 20 MHz and need a VCO frequency that will be able to support 122.88MHz and 245.76 outputs. If this is the case, yes it is possible and should work fine. Here is an example:
Regards,
Will