This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC555-Q1: Minimum time for the Trigger input to be at low

Part Number: TLC555-Q1
Other Parts Discussed in Thread: TLC555

Hi,

I would like to use TLC555 in monostable operation. I have below questions regarding the IC

1. What is the minimum time that trigger input to be low or less than trigger level to generate the Mono shot pulse ? where can i find this infromation in the datasheet ?

2. Once the threshold pin voltage reaches more than threshold level, the flip flop will be reset and the output is low. what will happen if there as a trigger pulse before the timing capacitor completely discharges through discharge FET ?