This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Output Synchronization & Sysreq_req

Part Number: LMX2594
Other Parts Discussed in Thread: LMK04832,

Hi,

We are using LMX2594 with LMK04832 and ADC12DJ5200

We have sysref_req through LMK04832 SDCLKOUT as shown below,

LMK 

LMX

OSCIN-100MHz, RFOutA&B-3.2GHz, SYSREF_REQ-5MHz,

SYNC pin is not used currently, but there is an option to drive from FPGA.

  1. What output standard should be set for SYSREF_REQ?
  2. To synchronization LMX2594, what are the steps to be followed?
    1. VCO_PHASE_SYNC should be enabled?
    2. MASH_RESET should be enabled?
    3. MASH_SEED_EN should be enabled?

Can you please suggest what Mash & Phase synchronization values to be set.

Thanks.

  • Hi There,

    Your configuration is a Cat. 1 sync, you don't need to set VCO_PHASE_SYNC = 1. 

    MASH_SEED is not related to phase sync, leave it = 0.

    You have set MASH_ORDER = 0, please set PFD_DLY_SEL accordingly. See Table 2 in the datasheet for details.

  • Hi Noel Fung

    Thanks for your answer.

    Can you please explain what should be done for the RFOutA and RFOutB synchronization outputs? General settings/config setting for LMX2594 Output synchronization? 

    Please answer to this also,

    1. What output standard should be set for SYSREF_REQ? of LMK04832?
  • Hi There,

    There is nothing to do with RFoutA, RFoutB and SYSREFREQ because your configuration is Cat.1 sync. I was wrong in the previous thread, you need to put VCO_PHASE_SYNC = 1 because you are using the CHDIV. No SYNC pulse is needed in Cat.1 sync configuration, phase will always aligned after programming.

    LMX2594 SYNC pin accepts LVDS and CMOS, I suggest use CMOS  for simplicity. INPIN_IGNORE bit should =0 to enable SYNC pin. 

  • Hi

    Is it possible for you to share the tics file? with setting mentioned above?

    Note that for the SYSREF_REQ pin from LMK04832, we have series AC Caps and then setting is done for CMOS. That should be fine right?

    SYNC is not driven.

    Thanks.

  • Hi There

    Your configuration is already correct, expect that you should set PFD_DLY_SEL accordingly.

    If it is a CMOS output, we should make it DC-couple. 

  • i

    Thanks.

    Can you please explain whether SYSREF_REQ has to be applied for LMX2594 Output RFOutA & RFOutB synchronization. Or just the VCO_PHASE_SYNC is enough?

    Please clarify.

    When we set VCO_PHASE_SYNC enabled in LMX2594, We are not able to see the LMX2594 Lock (Through MUXOUT register).

    I've attached the both LMX2594 and LMK04832 file, please check the files once and let us know anything to be changed.

    Goal is to Synchronize all the LMK04832 Outputs and LMX2594 Output synchronization

     

    LMX2594 RFOutA&B 3200MHz

    LMK config:

    mwr -force 0x10220000  0x000090; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000010; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000306; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000463; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x0005D1; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000670; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000C51; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000D04; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010014; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01010A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010340; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x010420; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010711; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010804; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01090A; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x010A00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010B40; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010E01; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010F04; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011020; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01110A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011340; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011420; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011744; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011814; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01190A; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011A00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011B40; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011E01; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011FF1; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012020; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01210A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012340; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x012420; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012714; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012808; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x01290A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012A00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012B40; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012D00; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x012E01; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012F10; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013014; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01310A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013340; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x013420; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013711; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013825; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013903; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013A02; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x013B80; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013C00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013D08; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013E03; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013F0D; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01400B; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014100; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014311; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x0144FF; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014608; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01470A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014802; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014942; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014A03; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014B06; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014C00; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x014D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014EC0; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014F7F; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x015001; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015102; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015300; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01540A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015608; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015700; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015896; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015900; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015A05; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015BD4; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x015C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015E1E; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015F0B; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016000; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016101; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01624D; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016300; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016400; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01650C; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x016958; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016A20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016B00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016C00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016E13; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x017310; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x017700; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x018200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x018300; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016600; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x016700; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016808; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x055500; mwr -force 0x10220004 0x1;

    LMX

    R112	0x700000
    R111	0x6F0000
    R110	0x6E0000
    R109	0x6D0000
    R108	0x6C0000
    R107	0x6B0000
    R106	0x6A0000
    R105	0x690021
    R104	0x680000
    R103	0x670000
    R102	0x663F00
    R101	0x650011
    R100	0x640000
    R99	0x630000
    R98	0x620400
    R97	0x610888
    R96	0x600000
    R95	0x5F0000
    R94	0x5E0000
    R93	0x5D0000
    R92	0x5C0000
    R91	0x5B0000
    R90	0x5A0000
    R89	0x590000
    R88	0x580000
    R87	0x570000
    R86	0x560000
    R85	0x55B200
    R84	0x540001
    R83	0x530000
    R82	0x524800
    R81	0x510000
    R80	0x50CCCC
    R79	0x4F004C
    R78	0x4E0003
    R77	0x4D0000
    R76	0x4C000C
    R75	0x4B0840
    R74	0x4A0000
    R73	0x49003F
    R72	0x480001
    R71	0x470085
    R70	0x46C350
    R69	0x450000
    R68	0x4403E8
    R67	0x430000
    R66	0x4201F4
    R65	0x410000
    R64	0x401388
    R63	0x3F0000
    R62	0x3E0322
    R61	0x3D00A8
    R60	0x3C0000
    R59	0x3B0001
    R58	0x3A9001
    R57	0x390020
    R56	0x380000
    R55	0x370000
    R54	0x360000
    R53	0x350000
    R52	0x340820
    R51	0x330080
    R50	0x320000
    R49	0x314180
    R48	0x300300
    R47	0x2F0300
    R46	0x2E07FC
    R45	0x2DC0DF
    R44	0x2C1F20
    R43	0x2B0000
    R42	0x2A0000
    R41	0x290000
    R40	0x280000
    R39	0x2703E8
    R38	0x260000
    R37	0x250204
    R36	0x240020
    R35	0x230004
    R34	0x220000
    R33	0x211E21
    R32	0x200393
    R31	0x1F43EC
    R30	0x1E318C
    R29	0x1D318C
    R28	0x1C0488
    R27	0x1B0002
    R26	0x1A0DB0
    R25	0x190C2B
    R24	0x18071A
    R23	0x17007C
    R22	0x160001
    R21	0x150401
    R20	0x14E048
    R19	0x1327B7
    R18	0x120064
    R17	0x11012C
    R16	0x100080
    R15	0x0F064F
    R14	0x0E1E70
    R13	0x0D4000
    R12	0x0C5001
    R11	0x0B0018
    R10	0x0A10D8
    R9	0x090604
    R8	0x082000
    R7	0x0740B2
    R6	0x06C802
    R5	0x0500C8
    R4	0x040A43
    R3	0x030642
    R2	0x020500
    R1	0x010808
    R0	0x00641C
    

  • Hi There,

    I don't have problem making the LMX devices to lock with your configuration file. Please note our programming recommendation is, first of all, program all the registers in descending order. Wait for 10ms then program R0 one more time.

    After programming the LMX devices, since it is a Cat.1 sync, all LMX devices outputs will be in phase. Below is the result using the LMX2594PSEVM. 

    SYSREFREQ is used for sysref generation, not phase synchronization. If it is a Cat.3 sync then we need to feed a time critical sync pulse to the SYNC pin. 

    Please provide LMK device configuration file in TICS Pro format, I will review it.

  • I'm not able to attach TCL file here

  • Hi Noel Fung,

    Please find the attached TCL file for LMK04832. In accordance with KLN's recommendation

    mwr -force 0x10220000  0x000090; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000010; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000306; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000463; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x0005D1; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000670; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000C51; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x000D04; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010014; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01010A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010340; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x010420; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010711; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010804; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01090A; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x010A00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010B40; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010E01; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x010F04; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011020; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01110A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011340; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011420; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011744; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011814; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01190A; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011A00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011B40; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x011E01; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x011FF1; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012020; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01210A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012340; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x012420; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012714; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012808; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x01290A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012A00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012B40; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012D00; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x012E01; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x012F10; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013014; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01310A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013340; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x013420; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013601; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013711; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013825; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013903; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013A02; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x013B80; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013C00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013D08; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013E03; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x013F0D; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01400B; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014100; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014311; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x0144FF; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014608; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01470A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014802; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014942; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014A03; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014B06; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014C00; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x014D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014EC0; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x014F7F; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x015001; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015102; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015300; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01540A; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015500; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015608; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015700; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015896; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015900; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015A05; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015BD4; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x015C20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015E1E; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x015F0B; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016000; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016101; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01624D; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016300; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016400; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x01650C; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x016958; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016A20; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016B00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016C00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016D00; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016E13; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x017310; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x017700; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x018200; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x018300; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016600; mwr -force 0x10220004 0x1;
    after 100
    mwr -force 0x10220000  0x016700; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x016808; mwr -force 0x10220004 0x1;
    mwr -force 0x10220000  0x055500; mwr -force 0x10220004 0x1;

  • Hello,

    We are out of office for a US holiday. Please expect a response by Monday.

    Thanks,

    Kadeem

  • Hi Ganesh,

    After configurating TICS Pro, in the menu bar, click File --> Save

    TICS Pro will save a file with .tcs extension. 

    To attach a file in E2E, 

    Click Upload and select the saved .tcs file.

  • Hi

    How do we synch/Phase align OSCIN of LMX2594 with RFOutx

  • Hi KLN, 
    The procedure depends on which category of SYNC you need for you application. 

    Please refer to the following snippet for the procedure: 

    Regards, 

    Vicente

  • Hi

    We will be working in Cat1 Sync required, CHDIV=2

    I do not see any Cat1 sync description in the sync procedure

  • Hi KLN, 
    If operating in Cat 1 - VCO phase sync must just be set to one and kept at 1 - not toggled. No further action is required on your part. 

    Regards, 

    Vicente

  • What about SYNC Pin driving?

    It's different from your saying to the drawing

  • You can also use the SYNC pin. Not an issue. 

    Regards, 

    Vicente