This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5010: TPL5010 USR Guide

Part Number: TPL5010

Tool/software:

Hi all,

This is Arabella, the FAE from NWC MM team. Now my customer used TPL5010 to data exchange project. There are 4 questions they want to know:

1. The customer did not use WAKE, and gave several high levels to DONE in 1S. Is this reasonable?
2. The timing is 6 minutes. During this period, how many high pulses does DONE give in 1s? Does this pin also serve as an LED indicator?
3. Does DONE have any requirements for pulse width? I saw in the PDF that the minimum is 100ns, but the maximum value is not mentioned.
4. Is it enough to give a high level once in 6 minutes?

Many thanks!

BS,

Arabella Zhang