Part Number: BQ32000
Tool/software:
Hi
Our product uses this RTC IC, and it has already been implemented in a large volume of mass-produced products.
Currently, we are encountering an issue with a new model, but the RTC circuitry, layout routing, test flow, and firmware have not been changed.
However, during testing, it seems that the charging behavior does not achieve the trickle charge function. we would like to know,
1. Is the default setting of this IC configured to follow the path mentioned below when it leaves the factory?

2. When we read the registers through I2C, the values are as follows:
0x08 value: 0x20
0x09 value: 0x05
These values appear to be the default values set in our firmware, but they don't seem to be functioning as expected.
it seems that we need to reset them in order to enable the trickle charge,
3. When we write the actual time, what voltage is required to retain this time after a system reset?
currently, we are encountering a situation where the time is lost after a reset when the voltage is above 1.4V.
It seems that a voltage of around 1.6V or higher is needed to retain the actual time.
but the SPEC mentioned the Vback operating range is between 1.4V to 2.0V, is it reasonable?
as the above questions, we would like to know is there any possible to caused this phenomenon even we didn't modify any part,