This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS542A50: output voltage setting

Part Number: TPS542A50
Other Parts Discussed in Thread: TPS544C26

Tool/software:

Hi,

I have some questions about TPS542A50.

1. Does TPS542A50 output voltage only can adjust from m –20% to +10%? If my default voltage is 0.5V. TPS542A50 can't rise up voltage to 0.85V?

2. Set VSET = 0.1V to let output voltage =0.5V, it when IC enable, it will output default 0.5V, right?

3. Is there have other suggestion if I need Vin=12V Vout= 0.5V~0.85V(control by I2C)(adjust per level <25mV), need set default output =0.5V, Iout= 4A, there have any better suggestion?

Thanks!

Jeff