This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04101: PLL1 of the clock generator is not locking

Part Number: LMK04101


Tool/software:

The clock generator I am using has two PLLs. PLL2 is perfectly locking but not PLL1.
Below is my desired frequency setting for the clk. gen. 
PLL1: 

PLL2: 

We used recommended design for loop filter at first, that is

Later tried with increased bandwidth to 17kHz but that also did not help


Not really able to understand why PLL1 is not locking. Please help